Performs processing in response to detection of overrun error.
This API function is called as the callback routine of interrupt process r_dalin_interrupt_receive corresponding to the DALI reception end interrupt INTSRDLn (process performed when the amount of data received is greater than the argument rx_num specified for R_DALIn_Receive). |
uint16_t rx_data; |
Receive data (greater than the argument rx_num specified for R_DALIn_Receive) |