r_intfo_interrupt


Performs processing in response to the external maskable interrupt INTFO.

Remark

This API function is called as the interrupt process corresponding to the external maskable interrupt INTFO.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_intfo_interrupt ( void );

 

CC-RL Compiler

[Argument(s)]

static  void  __near r_intfo_interrupt ( void );

None.

[Return value]

None.