3.2.38
Interrupt functions
Below is a list of API functions output by the Code Generator for interrupt functions use.
Table 3.38 | API Functions: [Interrupt Functions] |
|
|
|
|
R_INTC_Create
|
Performs initialization necessary to control the interrupt functions.
|
|
R_INTC_Create_UserInit
|
Performs user-defined initialization relating to the interrupt functions.
|
|
r_intcn_interrupt
|
Performs processing in response to the external maskable interrupt INTPn.
|
|
R_INTCn_Start
|
Enables the acceptance of the external maskable interrupts INTPn.
|
|
R_INTCn_Stop
|
Disables the acceptance of the external maskable interrupts INTPn.
|
|
r_intclrn_interrupt
|
Performs processing in response to the external maskable interrupt INTPLRn.
|
|
R_INTCLRn_Start
|
Enables the acceptance of the external maskable interrupts INTPLRn.
|
|
R_INTCLRn_Stop
|
Disables the acceptance of the external maskable interrupts INTPLRn.
|
|
r_intrtcicn_interrupt
|
Performs processing in response to the external maskable interrupt INTRTCICn.
|
|
R_INTRTCICn_Start
|
Enables the acceptance of the external maskable interrupts INTRTCICn.
|
|
R_INTRTCICn_Stop
|
Disables the acceptance of the external maskable interrupts INTRTCICn.
|
|
R_INTFO_Start
|
Enables the acceptance of the external maskable interrupts INTFO.
|
|
R_INTFO_Stop
|
Disables the acceptance of the external maskable interrupts INTFO.
|
|
R_INTFO_ClearFlag
|
Clears INTFCLR flag of Interrupt flag output control register 1 (INTFOCTL1).
|
|
r_intfo_interrupt
|
Performs processing in response to the external maskable interrupt INTFO.
|