R_IT8bitm_Channeln_Set_PowerOff
|
Halts the clock supplied to the 8-bit interval timer.
Remark | Calling this API function changes the 8-bit interval timer to reset status.
For this reason, writes to the control registers after this API function is called are ignored.
|
[Syntax]
void R_IT8bitm_Channeln_Set_PowerOff ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.