3.2.17 16-bit wakeup timer

Below is a list of API functions output by the Code Generator for 16-bit wakeup timer (WUTM) use.

Table 3.17

API Functions: [16-bit Wakeup Timer]

API Function Name

Function

R_WUTM_Create

Performs initialization necessary to control the 16-bit wakeup timer.

R_WUTM_Create_UserInit

Performs user-defined initialization relating to the 16-bit wakeup timer.

r_wutm_interrupt

Performs processing in response to the timer interrupt.

R_WUTM_Start

Starts the count for 16-bit wakeup timer.

R_WUTM_Stop

Ends the count for 16-bit wakeup timer.

R_WUTM_Set_PowerOff

Halts the clock supplied to the 16-bit wakeup timer.