r_lvd_vbatinterrupt


Performs processing in response to the voltage detection of VBAT pin interrupt INTLVDVBAT.

Remark

This API function is called as the interrupt process corresponding to the voltage detection of VBAT pin interrupt INTLVDVBAT.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_lvd_vbatinterrup ( void );

 

CC-RL Compiler

static  void  __near r_lvd_vbatinterrup ( void );

[Argument(s)]

None.

[Return value]

None.