r_lvd_exlvdinterrupt


Performs processing in response to the voltage detection of EXLVD pin interrupt INTLVDEXLVD.

Remark

This API function is called as the interrupt process corresponding to the voltage detection of EXLVD pin interrupt INTLVDEXLVD.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_lvd_exlvdinterrup ( void );

 

CC-RL Compiler

static  void  __near r_lvd_exlvdinterrup ( void );

[Argument(s)]

None.

[Return value]

None.