|
R_TAUm_Channeln_Lower8bits_Start
|
Starts the count (lower 8-bit) for channel n.
Remarks 1. | This API function can only be called when the timer array unit is used as a 8-bit timer. |
Remarks 2. | The time from the call to this API function to the start of counting depends on the type of the function in question (e.g. interval timer, external event counter, or delay counter). |
[Syntax]
void R_TAUm_Channeln_Lower8bits_Start ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.