Renesas Electronics
Below is a list of API functions output by the Code Generator for timer array unit use.
Table 3.5
API Functions: [Timer Array Unit]
API Function Name
Function
R_TAUm_Create
Performs initialization necessary to control the timer array unit.
R_TAUm_Create_UserInit
Performs user-defined initialization relating to the timer array unit.
r_taum_channeln_interrupt
Performs processing in response to the timer interrupt INTTMmn.
r_taum_channeln_higher8bits_interrupt
Performs processing in response to the timer interrupt INTTMmnH.
R_TAUm_Channeln_Start
Starts the count for channel n.
R_TAUm_Channeln_Higher8bits_Start
Starts the count (higher 8-bit) for channel n.
R_TAUm_Channeln_Lower8bits_Start
Starts the count (lower 8-bit) for channel n.
R_TAUm_Channeln_Stop
Ends the count for channel n.
R_TAUm_Channeln_Higher8bits_Stop
Ends the count (higher 8-bit) for channel n.
R_TAUm_Channeln_Lower8bits_Stop
Ends the count (lower 8-bit) for channel n.
R_TAUm_Reset
Reset the timer array unit.
R_TAUm_Set_PowerOff
Halts the clock supplied to the timer array unit.
R_TAUm_Channeln_Get_PulseWidth
Captures the high/low-level width measured between pulses of the signal (pulses) input to the TImn pin.
R_TAUm_Channeln_Set_SoftwareTriggerOn
Generates the trigger (software trigger) for one-shot pulse output.