R_KB2m_TKBOn0_SmoothStartFunction_Stop
|
Ends smooth start function for timer output TKBOn0.
[Syntax]
void R_KB2m_TKBOn0_SmoothStartFunction_Stop ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.