|
|
R_KB2m_Create
|
Performs initialization necessary to control the 16-bit timer KB2.
|
R_KB2m_Create_UserInit
|
Performs user-defined initialization relating to the 16-bit timer KB2.
|
r_kb2m_interrupt
|
Performs processing in response to the timer interrupt INTTKB2m.
|
R_KB2m_Start
|
Starts the count for 16-bit timer KB2.
|
R_KB2m_Stop
|
Ends the count for 16-bit timer KB2.
|
R_KB2m_Set_PowerOff
|
Halts the clock supplied to the 16-bit timer KB2.
|
R_KB2m_Simultaneous_Start
|
Starts the simultaneous start/stop mode.
|
R_KB2m_Simultaneous_Stop
|
Ends the simultaneous start/stop mode.
|
R_KB2m_Synchronous_Start
|
Starts the timer start/clear mode.
|
R_KB2m_Synchronous_Stop
|
Ends the timer start/clear mode.
|
R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Start
|
Starts forced output stop function 1 for timer output TKBOn0.
|
R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Stop
|
Ends forced output stop function 1 for timer output TKBOn0.
|
R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start
|
Starts forced output stop function 2 for timer output TKBOn1.
|
R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Stop
|
Starts forced output stop function 2 for timer output TKBOn1.
|
R_KB2m_TKBOn0_DitheringFunction_Start
|
Starts dithering function for timer output TKBOn0.
|
R_KB2m_TKBOn0_DitheringFunction_Stop
|
Ends dithering function for timer output TKBOn0.
|
R_KB2m_TKBOn1_DitheringFunction_Start
|
Starts dithering function for timer output TKBOn1.
|
R_KB2m_TKBOn1_DitheringFunction_Stop
|
Ends dithering function for timer output TKBOn1.
|
R_KB2m_TKBOn0_SmoothStartFunction_Start
|
Starts smooth start function for timer output TKBOn0.
|
R_KB2m_TKBOn0_SmoothStartFunction_Stop
|
Ends smooth start function for timer output TKBOn0.
|
R_KB2m_TKBOn1_SmoothStartFunction_Start
|
Starts smooth start function for timer output TKBOn1.
|
R_KB2m_TKBOn1_SmoothStartFunction_Stop
|
Ends smooth start function for timer output TKBOn1.
|
R_KB2m_Set_BatchOverwriteRequestOn
|
Enables batch overwriting of the compare register.
|