R_TMRJ0_Create_UserInit


Performs user-defined initialization relating to the 16-bit timer RJ0.

Remark

This API function is called as the R_TMRJ0_Create callback routine.

[Syntax]

void    R_TMRJ0_Create_UserInit ( void );

[Argument(s)]

None.

[Return value]

None.