3.2.6 Timer RJ

Below is a list of API functions output by the Code Generator for timer RJ use.

Table 3.6

API Functions: [Timer RJ]

API Function Name

Function

R_TMR_RJ0_Create

Performs initialization necessary to control the 16-bit timer RJ0.

R_TMR_RJ0_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RJ0.

r_tmr_rj0_interrupt

Performs processing in response to the timer interrupt.

R_TMR_RJ0_Start

Starts the count for 16-bit timer RJ0.

R_TMR_RJ0_Stop

Ends the count for 16-bit timer RJ0.

R_TMR_RJ0_Set_PowerOff

Halts the clock supplied to the 16-bit timer RJ0.

R_TMR_RJ0_Get_PulseWidth

Reads the pulse width of the 16-bit timer RJ0.

R_TMRJ0_Create

Performs initialization necessary to control the 16-bit timer RJ0.

R_TMRJ0_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RJ0.

r_tmrj0_interrupt

Performs processing in response to the timer interrupt.

R_TMRJ0_Start

Starts the count for 16-bit timer RJ0.

R_TMRJ0_Stop

Ends the count for 16-bit timer RJ0.

R_TMRJ0_Set_PowerOff

Halts the clock supplied to the 16-bit timer RJ0.

R_TMRJ0_Get_PulseWidth

Reads the pulse width of the 16-bit timer RJ0.