Halts the clock supplied to the 16-bit wakeup timer.
Remark | Calling this API function changes the 16-bit wakeup timer to reset status.
For this reason, writes to the control registers after this API function is called are ignored.
|
[Syntax]
void R_WUTM_Set_PowerOff ( void );
|
[Argument(s)]
None.
[Return value]
None.