Performs processing in response to the comparator B interrupt.
Remark | This API function is called to run interrupt processing for the comparator Bn interrupt, which is generated when the comparison result changes at this time. |
[Syntax]
void r_cmpb_cmpbn_interrupt ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.