3.2.33 Comparator B (CMPB)

Below is a list of API functions output by the Code Generator for Comparator B use.

Table 3.33

API Functions: [Comparator B]

API Function Name

Function

R_CMPB_Create

Performs initialization necessary to control the Comparator B.

R_CMPB_Create_UserInit

Performs user-defined initialization relating to the Comparator B.

r_cmpb_cmpbn_interrupt

Performs processing in response to the comparator B interrupt.

R_CMPBn_Start

Starts comparison for analog input voltage.

R_CMPBn_Stop

Ends comparison for analog input voltage.