Performs processing in response to the overflow interrupt.
Remark | This API function is called to run interrupt processing for the overflow interrupt, which is generated in response to an overflow of the timer counter (TCNT). |
[Syntax]
static void r_mtu2_tcivn_interrupt ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.