Renesas Electronics
Below is a list of API functions output by the Code Generator for multi-function timer pulse unit 2 use.
Table 3.12
API Functions: [Multi-Function Timer Pulse Unit 2]
API Function Name
Function
R_MTU2_Create
Performs initialization necessary to control the multi-function timer pulse unit 2.
R_MTU2_Create_UserInit
Performs user-defined initialization relating to the multi-function timer pulse unit 2.
r_mtu2_tgimn_interrupt
Performs processing in response to the input capture/compare match interrupt.
r_mtu2_cj_tgimn_interrupt
r_mtu2_tcivn_interrupt
Performs processing in response to the overflow interrupt.
r_mtu2_cj_tcivn_interrupt
r_mtu2_tciun_interrupt
Performs processing in response to the underflow interrupt.
R_MTU2_Cn_Start
Starts counting by a 16-bit timer.
R_MTU2_Cn_Stop
Ends counting by a 16-bit timer.