Renesas Electronics
R_MTU3_Create_UserInit
Performs user-defined initialization relating to the multi-function timer pulse unit 3.
Remark
This API function is called as the R_MTU3_Create callback routine.
[Syntax]
void R_MTU3_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]