3.2.13 Multi-function timer pulse unit 3 (MTU3)

Below is a list of API functions output by the Code Generator for multi-function timer pulse unit 3 use.

Table 3.13

API Functions: [Multi-Function Timer Pulse Unit 3]

API Function Name

Function

R_MTU3_Create

Performs initialization necessary to control the multi-function timer pulse unit 3.

R_MTU3_Create_UserInit

Performs user-defined initialization relating to the multi-function timer pulse unit 3.

r_mtu3_tgimn_interrupt

Performs processing in response to the input capture/compare match interrupt.

r_mtu3_cj_tgimn_interrupt

Performs processing in response to the input capture/compare match interrupt.

r_mtu3_tcivn_interrupt

Performs processing in response to the overflow interrupt.

r_mtu3_cj_tcivn_interrupt

Performs processing in response to the overflow interrupt.

r_mtu3_tciun_interrupt

Performs processing in response to the underflow interrupt.

R_MTU3_Cn_Start

Starts counting by a 16-bit timer.

R_MTU3_Cn_Stop

Ends counting by a 16-bit timer.