R_RIICn_StartCondition


Issues the start condition and causes a transfer error and an event generation interrupt (EEI).

Remarks 1.

This API function is called as the internal function of R_RIICn_Master_Send and R_RIICn_Master_Receive.

Remarks 2.

r_riicn_error_interrupt is called in response to calling of this API function.

[Syntax]

void    R_RIICn_StartCondition ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.