r_riicn_callback_receiveerror


Of the internal processing for transfer errors and event generation interrupts (EEI), this function handles processing specialized in the arbitration-lost detection, NACK detection, and timeout detection.

Remark

This API function is called as the r_riicn_error_interrupt callback routine.

[Syntax]

#include    "r_cg_macrodriver.h"
static  void    r_riicn_callback_receiveerror ( MD_STATUS status );

Remark

n is the channel number.

[Argument(s)]

I/O

Argument

Description

I

MD_STATUS status;

Source of the transfer errors and event generation interrupts

MD_ERROR1: Arbitration-lost detection

MD_ERROR2: Timeout detection

MD_ERROR3: NACK detection

[Return value]

None.