Starts RSPI transmission/reception.
This API function repeats RSPI transmission in byte units the number of times specified by the argument tx_num from the buffer at the location specified by the argument tx_buf. |
This API function repeats RSPI reception processing in byte units the number of times specified by the argument tx_num and then stores the received data in the buffer at the location specified by the argument rx_buf. |
When performing a RSPI transmission/reception, R_RSPIn_Start must be called before this API function is called. |
#include "r_cg_macrodriver.h" MD_STATUS R_RSPIn_Send_Receive ( uint8_t * const tx_buf, uint16_t tx_num, uint8_t * const rx_buf ); |