Performs processing in response to the RSPI error interrupts.
This API function is called as the r_rspin_error_interrupt callback routine. |
uint8_t err_type; |
Source of the RSPI error interrupt (x is undefined) xxxx00x1B: Overrun error detection |