Performs processing in response to the framing error or parity error interrupts.
Remark | This API function is called to run the interrupt processing for the framing error or parity error interrupt. |
[Syntax]
static void r_scifan_erif_interrupt ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.