r_scifan_drif_interrupt


Performs processing in response to the receive data ready interrupts.

Remark

This API function is called to run the interrupt processing for the receive data ready interrupt.

[Syntax]

static  void    r_scifan_drif_interrupt ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.