Renesas Electronics
18.2.13 Interrupt management functions The following shows the service calls provided by the RI600V4 as the interrupt management functions. Table 18-15 Interrupt Management Functions Service Call Function Useful Range chg_ims Change interrupt mask Task ichg_ims Change interrupt mask Non-task get_ims Reference interrupt mask Task iget_ims Reference interrupt mask Non-task