sus_tsk
isus_tsk
ER sus_tsk (ID tskid);ER isus_tsk (ID tskid);These service calls move the task specified by parameter tskid from the RUNNING state to the SUSPENDED state, from the READY state to the SUSPENDED state, or from the WAITING state to the WAITING-SUSPENDED state.
If the target task has moved to the SUSPENDED or WAITING-SUSPENDED state when this service call is issued, these service calls return "E_QOVR".