If a service call (
chg_pri,
sig_sem, etc.) accompanying dispatch processing is issued during the interval from when
dis_dsp is issued until this service call is issued, the RI78V4 executes only processing such as queue manipulation, counter manipulation, etc., and the actual dispatch processing is delayed until this service call is issued, upon which the actual dispatch processing is performed in batch.
Note This service call does not perform queuing of enable requests. If the system is in the dispatching enabled state, therefore, no processing is performed but it is not handled as an error.