-
frsm_tsk
ifrsm_tsk
-
Forcibly resume suspended task.
ER frsm_tsk ( ID tskid );
ER ifrsm_tsk ( ID tskid );
|
MOV A, #tskid
CALL !!_frsm_tsk
MOV A, #tskid
CALL !!_ifrsm_tsk
|
|
|
|
|
|
|
ID tskid;
|
ID number of the task to be resumed.
|
These service calls set the suspend request counter for the task specified by parameter
tskid to 0x1 f, and then forcibly cancel the SUSPENDED state of the target task.
As a result, the target task is moved from the SUSPENDED state to the READY state, or from the WAITING-SUSPENDED state to the WAITING state.
Note 1 If the target task is moved to the READY state after this service call is issued, this service call also re-queues the task at the end of the ready queue corresponding to the priority of the task.
Note 2 This service call does not perform queuing of forced cancellation requests. If the target task is in a state other than the SUSPENDED or WAITING-SUSPENDED state, "E_OBJ" is therefore returned.
|
|
|
|
|
|
|
|
|
|
|
Object state error (specified task is neither in the SUSPENDED state nor WAITING-SUSPENDED state).
|