-
rel_wai
irel_wai
-
Release task from waiting.
ER rel_wai ( ID tskid );
ER irel_wai ( ID tskid );
|
MOV A, #tskid
CALL !!_rel_wai
MOV A, #tskid
CALL !!_irel_wai
|
|
|
|
|
|
|
ID tskid;
|
ID number of the task to be released from waiting.
|
These service calls forcibly cancel the WAITING state of the task specified by parameter
tskid.
As a result, the target task unlinked from the wait queue and is moved from the WAITING state to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
"E_RLWAI" is returned from the service call that triggered the move to the WAITING state (
slp_tsk,
wai_sem, or the like) to the task whose WAITING state is cancelled by this service call.
Note 1 If the target task is moved to the READY state after this service call is issued, this service call also re-queues the task at the end of the ready queue corresponding to the priority of the task.
Note 2 This service call does not perform queuing of forced cancellation requests. If the target task is in a state other than the WAITING or WAITING-SUSPENDED state, "E_OBJ" is returned.
|
|
|
|
|
|
|
|
|
|
|
Object state error (specified task is neither in the WAITING state nor WAITING-SUSPENDED state).
|