-
twai_flg
-
Wait for eventflag (with timeout).
ER twai_flg ( ID flgid, FLGPTN waiptn, MODE wfmode, FLGPTN *p_flgptn, TMO tmout
);
|
MOVW AX, #tmout_hi
PUSH AX
MOVW AX, #tmout_lo
PUSH AX
MOVW DE, #LOWW(_p_flgptn)
MOVW BC, #waiptn
MOVW AX, #(flgid | wfmode)
CALL !!_twai_flg
addw sp, #0x0004
|
|
|
|
|
|
|
ID flgid;
|
ID number of the eventflag wait for.
|
|
|
FLGPTN waiptn;
|
Wait bit pattern (16 bits).
|
|
|
MODE wfmode;
|
TWF_ANDW: AND waiting condition.
TWF_ORW: OR waiting condition.
|
|
|
FLGPTN *p_flgptn;
|
Bit pattern causing a task to be released from waiting.
|
|
|
TMO tmout;
|
Specified timeout (unit: ticks).
TMO_FEVR: Waiting forever.
Value: Specified timeout.
|
This service call checks whether the bit pattern specified by parameter
waiptn and the bit pattern that satisfies the required condition specified by parameter
wfmode are set to the eventflag specified by parameter
flgid.
If the bit pattern that satisfies the required condition has been set to the target eventflag, the bit pattern of the target eventflag is stored in the area specified by parameter
p_flgptn.
If the bit pattern of the target eventflag does not satisfy the required condition when this service call is issued, the invoking task is queued to the target eventflag wait queue.
As a result, the invoking task is unlinked from the ready queue and is moved from the RUNNING state to the WAITING state (waiting state for an eventflag).
The waiting state for an eventflag is cancelled in the following cases, and then moved to the READY state.
Waiting State for an Eventflag Cancel Operation
|
|
A bit pattern that satisfies the required condition was set to the target eventflag as a result of issuing set_flg.
|
|
A bit pattern that satisfies the required condition was set to the target eventflag as a result of issuing iset_flg.
|
|
Forced release from waiting (accept rel_wai while waiting).
|
|
Forced release from waiting (accept irel_wai while waiting).
|
|
Polling failure or timeout.
|
|
The following shows the specification format of required condition
wfmode.
-
wfmode = TWF_ANDW
Checks whether all of the bits to which 1 is set by parameter
waiptn are set as the target eventflag.
-
wfmode = TWF_ORW
Checks which bit, among bits to which 1 is set by parameter
waiptn, is set as the target eventflag.
Note 1 In the RI78V4, the number of tasks that can be queued to the eventflag wait queue is one. If this service call is issued for the eventflag to which a task is queued, therefore, "E_ILUSE" is returned regardless of whether or not the required condition is immediately satisfied.
Note 2 The RI78V4 performs bit pattern clear processing (0x0 setting) when the required condition of the target eventflag (TA_CLR attribute) is satisfied.
Note 3 When TMO_FEVR is specified for wait time tmout, processing equivalent to
wai_flg will be executed. When TMO_POL is specified, processing equivalent to
pol_flg will be executed.
|
|
|
|
|
|
|
|
|
|
|
Illegal service call use (there is already a task waiting for an eventflag with the TA_WSGL attribute).
|
|
|
|
|
|
|
|
Polling failure or timeout.
|