5.1.7 Byte separation operators

The following byte separation operators are available.

Operator

Overview

HIGH

Returns the high-order 8-bit value of a term.

LOW

Returns the low-order 8-bit value of a term.