5.1.9 Section operators

The following section operators are available.

 

Operator

Overview

STARTOF

Returns the start address of the term section after linking.

SIZEOF

Returns the size of the term section after linking.