2.2.1 Select item

The resource information tool enables you to select the items to display in the Realtime OS Resource Information panel.

To select which items are displayed, right click on the header (header column or row) in the Realtime OS Resource Information panel, and from the context menu that appears, select "Display".

Figure 2-1. Select Item



Remark Select items to display by selecting their checkboxes.

Table 2-1. Select Item

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.