2.3 Confirm Resource Information

Check the resource information when program execution is stopped via the various tabs of the Realtime OS Resource Information panel (e.g. [System] tab and [Memory Area] tab).

The Realtime OS Resource Information panel is made up of the following tabs.

- [System] tab

- [Memory Area] tab

- [Task] tab

- [Semaphore] tab

- [Eventflag] tab

- [Data Queue] tab

- [Mailbox] tab

- [Fixed-Sized Memory Pool] tab

- [Cyclic Handler] tab

- [Interrupt Handler] tab

- [Initialize Routine] tab

- [Ready Queue] tab

- [Timer Queue] tab

Remark Switch tabs in the tab selection area of the Realtime OS Resource Information panel.[Interrupt Handler] tab