2.3.2 [Full-spec emulator]

Configure the operating environment on the Property panel below when using Full-spec emulator.

Figure 2.6

Example of Property Panel [Full-spec emulator]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.2.1 [Connect Settings] tab

2.3.2.2 [Debug Tool Settings] tab

2.3.2.3 [Download File Settings] tab

2.3.2.4 [Flash Options Settings] tab

2.3.2.5 [Hook Transaction Settings] tab