Configure the operating environment on the Property panel below when using E20.
Follow the steps below by selecting the corresponding tab on the Property panel.
2.3.4.1 [Connect Settings] tab
2.3.4.2 [Debug Tool Settings] tab
2.3.4.3 [Download File Settings] tab