Renesas Electronics
top
Debug Tool
FUNCTIONS
Preparation before Debugging
2.2 Preparation before Debugging
This section describes the preparation to start debugging the created program.
Previous Topic
Overview
Next Topic
Confirm the connection to a host machine
Table of Contents
Overview
Preparation before Debugging
Confirm the connection to a host machine
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Download/Upload Programs
Display/Change Programs
Select a Core (PE)
Execute Programs
Stop Programs (Break)
Display/Change the Memory, Register and Variable
Display Information on Function Call from Stack
Collect Execution History of Programs
Measure Execution Time of Programs
Measure Performance [Full-spec emulator][E1][E20]
Measure Coverage [Simulator]
Set an Action into Programs
Manage Events
Use Hook Function
About Input Value
Exclusive control checking tool
Pseudo-error debugging [Full-spec emulator][E1][E20]
Debugging CAN bus reception procedures [Full-spec emulator][E1][E20]