Renesas Electronics
top
Debug Tool
FUNCTIONS
Set an Action into Programs
2.16
Set an Action into Programs
This section describes how to set the specified action into the program.
Previous Topic
Display the coverage measurement result
Next Topic
Inset printf
Table of Contents
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Download/Upload Programs
Display/Change Programs
Select a Core (PE)
Execute Programs
Stop Programs (Break)
Display/Change the Memory, Register and Variable
Display Information on Function Call from Stack
Collect Execution History of Programs
Measure Execution Time of Programs
Measure Performance [Full-spec emulator][E1][E20]
Measure Coverage [Simulator]
Set an Action into Programs
Inset printf
Manage Events
Use Hook Function
About Input Value
Exclusive control checking tool
Pseudo-error debugging [Full-spec emulator][E1][E20]
Debugging CAN bus reception procedures [Full-spec emulator][E1][E20]