2.17.6.2
Event types that can be set and deleted during execution
The following types of events can be set or deleted during program execution, or during tracer/timer execution.
Table 2.21 | Event Types That Can be Set and Deleted during Execution |
|
|
|
|
|
|
|
|
Hardware Break
(execution type: after execution)
|
|
|
|
Hardware Break
(execution type: before execution)
|
|
|
|
Hardware Break
(access type)
|
|
|
|
Software Break
|
|
|
|
Trace
(trace start/trace end)
|
|
|
|
Point Trace
|
|
|
|
Timer Result
(timer start/timer end)
|
|
|
|
Performance Measurement
(performance measurement start/
performance measurement end)
|
|
|
|
Action
(Printf)
|
|
|
: Possible, if the program execution is allowed to pause for eventsNote
: Impossible while tracer or timer is executing
NG : Impossible
: Not supported
Note | To enable this, specify [Yes] with the [Set event by stopping execution momentarily] property in the [Set Event While Running] category on the [Debug Tool Settings] tab of the Property panel. |