| Events do not occur during step execution (including return execution) and program execution by selecting [Go to Here] from the context menu.  | 
| If the location set for an existing event changes to midway in an instruction because the program to debug has been downloaded again, re-set the event using the following method: | 
| When debugging information is available: | 
| When debugging information is not available: | 
| If a change to internal ROM/RAM changes the location the event is set to a non-mapped area, then set events will not occur (they will also not change to Invalid state /Suspended State on the Events panel). |