You configure the basic settings of the debug tool for each one of the following categories.
(2) [Access Memory While Running]
You can configure the memory in this category.
Current memory mapping status is displayed for each type of memory area.
You can configure the memory access while executing a program (the real-time display update function) in this category. See "2.9.1.4 Display/modify the memory contents during program execution" for details on the real-time display update function.
Select whether to automatically update the contents in the Memory panel/Watch panel display during a program execution.
Select [Yes] to update the display automatically (default).
The display contents of the Memory panel/Watch panel can be updated manually by clicking the |
This property is valid only when the [Update display during the execution] property is set to [Yes].
Specify the interval in 100ms unit to automatically update the contents in the Memory panel/Watch panel display while executing a program.
Directly enter the Integer number between 100 and 65500 (rounding up the fractions less than 100ms) (default: [500]).
You can configure the break function.
See "2.8 Stop Programs (Break)" for details on the break function and this category configuration.
You can configure the trace function in this category.
See "2.11 Collect Execution History of Programs" for details on the trace function and this category configuration.
You can configure the timer function in this category.
See "2.12 Measure Execution Time of Programs" for details on the timer function and this category configuration.
You can configure the coverage function in this category.
See "2.13 Measure Coverage [IECUBE][Simulator]" for details on the coverage function and this category configuration.
You can configure the Simulator GUI function in this category.
See "2.17 Use the Simulator GUI [Simulator]" for details on the Simulator GUI function and this category configuration.