This timer operation can be configured in the [Trace] category on the [Debug Tool Settings] tab in the Property panel. 
Figure 2.125  | [Timer] Category [Simulator]  | 
 
Select whether to use the timer function.
Select [Yes] to use the timer function (default: [No]).