Detailed Settings of Execution Events dialog box


This dialog box is used to display and change detailed information on execution-related events selected on the Events panel.

Note that the execution-related events refer to the following events on the Events panel.

-

Hardware break

-

After execution (or post-execution) break in the detailed information on combination break [E1] [E20] [EZ Emulator]

-

After execution (or post-execution) eventsNote registered as trace start and trace end events in the detailed information on trace

-

After execution (or post-execution) eventsNote registered as timer start and timer end events in the detailed information on timer result (or timer measurement)

Note

[Simulator]
Before execution (or pre-execution) events apply instead of after execution events.

Figure A.60

Detailed Settings of Execution Events Dialog Box

 

This section describes the following.

[How to open]

-

On the Events panel, move the caret to the hardware break of which you wish to change the detailed information, then select [Edit Condition ...] from the context menu.

-

On the Events panel, move the caret to the execution-related event in trace of which you wish to change the detailed information, then select [Edit Condition ...] from the context menu.

-

On the Events panel, move the caret to the execution-related event in timer result of which you wish to change the detailed information, then select [Edit Condition ...] from the context menu.

 

[E1] [E20] [EZ Emulator]

-

On the Events panel, move the caret to the execution-related event in combination break of which you wish to change the detailed information, then select [Edit Condition ...] from the context menu.

[Description of each area]

(1)

Detailed information display/change area

This area displays, in list form of the category, the detailed information on an execution-related event that is selected on the Events panel, allowing for its settings to be changed directly.

(2)

Property description area

This area displays a simple description of the category or property selected in the detailed information display/change area.

[Toolbar]

 

Displays a category in the detailed information display/change area.

 

Hides categories in the detailed information display/change area and rearranges only property items in the ascending order.

[Description of each category]

(1)

[Address]

Address

Display and specify the address at which an execution-related event is set.

Default

Depends on selected event

modifying

By entering directly from the keyboard

Available values

0x0 to 0xFFFFFFFF

(2)

[Pass Count]

Pass count

Specify a pass count in decimal.

The relevant event occurs when the event condition is met as many times as the entered pass count.

Default

1

Modifying

By entering directly from the keyboard

Available values

-

[E1] [E20] [EZ Emulator]

1 to 256

-

[Simulator]

1 to 16,383

Caution 1.

[E1] [E20] [EZ Emulator]
The pass count can be specified by any value other than 1 for only one event among all events (including access-related events).
If a pass count of other than 1 is specified for two events, an error results.

Caution 2.

[E1(Serial)/E20(Serial)/EZ Emulator [RX100, RX200 Series]]
No values other than 1 can be specified for the pass count.

[Function buttons]

Buttons

Functions

OK

Applies detailed settings made in this dialog box to execution-related events before closing the dialog box.

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.