When printing the content of the Disassemble panel, specify an address range of the subject to be printed.
This section describes the following.
On the Disassemble panel, choose [Print...] from the [File] menu. |
To specify a range to be printed, select one of the option buttons given below.
Prints only a currently displayed range on the Disassemble panel.
Prints only a currently selected range on the Disassemble panel.
However, this is disabled if nothing is selected on the Disassemble panel.
Specify an address range of the subject to be printed by [Start address] and [End address].
Enter an address expression directly in the respective text boxes (specifiable in up to 1,024 characters) or select an input history item from the drop-down list (up to 10 history entries).
By pressing the [Ctrl] + [Space] keys in this text box, it is possible to complement a symbol name at the current caret position (see "2.20.2 Symbol name completion function"). |
Closes this dialog box and opens a Windows printing dialog box to print a specified range of contents of the Disassemble panel. |
|