Renesas Electronics
top
Debug Tool
FUNCTIONS
Set an Action into Programs
2.16
Set an Action into Programs
This section describes how to set the specified action into the program.
Previous Topic
Display coverage measurement results
Next Topic
Insert printf
Table of Contents
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Download and Upload
Displaying and Changing Programs
Usage of PIC/PID Function
Setting Overlay Sections
Execute Programs
Stop Programs (Break)
Displaying and Changing Memory, Registers, and Variables
Display Function Call Information from the Stack
Collecting an Execution History
Measuring the Execution Time
Measure Coverage [Simulator] [E20 [RX71M and RX64M Groups]]
Set an Action into Programs
Insert printf
Insert an interrupt event [Simulator]
Event Management
Setting Up the Hook Process
Using the Debug Console
About Input Value
Differences between the Microcontroller and the Emulator
Other Notes on Usage [E1] [E20] [EZ Emulator]