2.16.2 Insert an interrupt event [Simulator]

Setting an interrupt event as one of the action events allows you to generate an interrupt at a desired location while the program is running. To use this function, follow the steps below.

 

2.16.2.1 Set an interrupt event

2.16.2.2 Execute the program

2.16.2.3 Edit interrupt event

 

Caution

Also see "2.17.7 Points to note regarding event setting" for details on interrupt event settings, including the allowable number of valid events.