Execute the program (see "2.9 Execute Programs").
When an instruction for which a timer start event or timer end event has been set is executed, a timer measurement is started or finished.
After execution of the program has stopped, the measurement result can be confirmed as a timer measurement event on the Events panel that is opened by choosing [Event] from the [View] menu, as shown below.
Note that this timer measurement event is a particular type of event that is displayed on only the Events panel when either a timer start event or a timer end event has been set.
Example of Measurement Results by Timer Measurement Event (Timer Start and End Events) [E1] [E20] |
Figure 2.161 Example of Measurement Results by Timer Measurement Event (Timer Start and End Events) |
Example of a Measurement Result by Timer Measurement Event (Timer Start and End Events) [Simulator] |