Renesas Electronics
To clear the content of the collected trace data, click the toolbar button .
However, this button is disabled while the trace function is in operation.
Remark
[Simulator] If you've selected [Yes] for the [Clear trace memory before running] property in the [Trace] category on the Property panel's [Debug Tool Settings] tab, the trace memory is cleared each time the program is run.